cancel
Showing results for 
Search instead for 
Did you mean: 

DynamicBitmapCreat in keil causes the program to enter a hardfault.

Louis__0
Associate III

I generated a Keil based TouchGFX project in stme2cubemx.The DynamicBitmapCreat function was called to create the first Bitmap without any problems, the ID and startAddress were all correct, but when I created the second Bitmap the program went straight into HardFault.I'm using TouchGFx16.0, and have used TouchGFx13.0 before, but have not resolved this issue.Any good suggestions?

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Romain DIELEMAN
ST Employee

Hi,

Could you edit the Topic tags to add the TouchGFX topic ? This will increase the visibility of your post.

/Romain

What kind of bill-of-goods did SalesForce sell you guys? Other forum software's have assignable / tiered moderation rights.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

In Keil make sure you have an adequate Heap defined in startup.s, and that is placed in the largest available RAM arena.

Have code sanity check pointers, and malloc() for NULL pointer returns when it runs out of resources.

Make sure to free() resources when done with them.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Sorry, this is my first post, I'm not familiar with it.

It doesn't seem to be the stack or RAM issue.I just found a way to solve this problem.

But why this should be done is unclear.

https://community.st.com/s/question/0D53W00000W92L3SAJ/firmware-crashes-with-dynamicbitmap-while-immigrating-from-touchgfx-4100-to-touchgfx-4150?t=1615438083524