STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

SPI2 in stm32f429 is not working while touchgfx and lcd config functions are added, however works fine if i comment the lcd config function and touchgfx init.

The lcd configuration uses LTDC(for data) and SPI5 for sending commands. The display driver used is ili9341. system clock configuration is as below./** * @brief System Clock Configuration *     The system Clock is configured as follow : *      System...

Eivor by Associate II
  • 2012 Views
  • 3 replies
  • 0 kudos

Resolved! SDMMC1 and LTDC on STM32H725/35

When configuring SDMMC1 in STM32CubeIDE, I get a warning that it conflicts with LTDC (RGB888). SDMMC2 does also conflict. Can someone guide me, how to resolve this conflict?

TRadd.1 by Associate II
  • 3060 Views
  • 7 replies
  • 0 kudos

How to use TouchGFX framebuffer to mirror x axis only

Long story short, I have a circular MIPI-DSI display and need to rotate the image by 180 deg. I've read the SW-only implementation post here, but it specifically mentions that this makes memory use highly inefficient, which is not ideal for our batte...

KDubo by Associate II
  • 1319 Views
  • 0 replies
  • 0 kudos

Resolved! C++ Strings Interpreted As Fallback Characters

I am using TGX v4.16.0. All of the work I describe with is with the TGX simulator in MSVS.I am building native C++ strings from C character arrays. I am then taking these strings and using them to update a single wildcard text area. Most of the te...

0693W00000Bbp5KQAR.png
CPaye.1 by Associate III
  • 1421 Views
  • 2 replies
  • 0 kudos

Resolved! Minimum space between frame buffers

Hello everyone,I'm currently developing a project using Touchgfx on a custom board with a STM32F469II, external RAM/FLASH, SD card and a 1024x600 screen.I'm having trouble placing the frame buffer in the external RAM close to eachover. Right now, the...

TDele.1 by Associate III
  • 2014 Views
  • 2 replies
  • 0 kudos