STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ethernet problem on STM32H747I-DISCO board

Hi everyone,I have a problem with the Ethernet connection that I can't solve on the STM32H747I-DISCO board.I followed Adam Berlinger's guide step by step (https://community.st.com/t5/stm32-mcus/how-to-create-a-project-for-stm32h7-with-ethernet-and-lw...

magianf by Associate
  • 26 Views
  • 0 replies
  • 1 kudos

Bidirectional Communication Between CM4 and CM7 Not Working on STM32H747I-DISCO (FreeRTOS Stream Buffer / Core Message Buffer)

  Working on bidirectional communication between CM4 and CM7 on the STM32H747I-DISCO using FreeRTOS stream buffers (CoreMessageBuffer). One-way communication works fine (either CM4 → CM7 or CM7 → CM4), but both directions at the same time do not work...

NUCLEO-G0B1RE with SNK1M1 only DEFAULT 5V

Hi STM32 community, I have ordered those the Evalboards: NUCLEO-G0B1RE X-NUCLEO-SNK1M1 - USB Type-C Power Delivery Sink  I have followed all of your existing applications, but none of the had lead to an similar result as displayed by your application...

kuda1311 by Associate
  • 111 Views
  • 1 replies
  • 0 kudos

Resolved! USB C PD Try.SRC and Try.SNK

I can't find Try.SRC or Try.SNK features for DRP devices in ST's USB C Power Delivery Stack (USBPD Core). Did I miss something?If it is not in the stack yet. Is ST planning to integrate this feature? What timeline are we looking at?Is it easy to impl...

abtq by Associate
  • 64 Views
  • 1 replies
  • 1 kudos