cancel
Showing results for 
Search instead for 
Did you mean: 

Problem to Flash STEVAL SPIN 3201 Board Example

JHenn.2
Associate

Hello,

I have a STEVAL-SPIN3201 board Rev 3.

Try to use the flash procedure from document UM2152

  • USB Connection to Windows 10 PC
  • 12V Power Supply to J2
  • Flash drive shows up with two files Fail.txt and Details.txt
  • I am able to delete the two files.
  • Windows shows a free memory of 24kB.
  • 12kB are always used.
  • Try to copy the SDK5x - STEVAL-SPIN3201 - BullRunning.bin example.
  • Windows refuses to copy because of insufficient space.

Is there any procedure to get the 12kB free?

Thanks in advance and best regards

Jens

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
JHenn.2
Associate

I found the problem... I had to update the STLINK SW on the board. This can be done with the STM32cubeProgrammer SW

View solution in original post

2 REPLIES 2
JHenn.2
Associate

I found the problem... I had to update the STLINK SW on the board. This can be done with the STM32cubeProgrammer SW

Laurent Ca...
Lead II

Dear @JHenn.2​ 

But you are welcome =) !

Best regards

Laurent Ca...