cancel
Showing results for 
Search instead for 
Did you mean: 

I can't compile a project created in X-CUBE-MCSDK-FUL_5. Y. 1 in the st-stm32cubeide environment.

АМикр.1
Associate

Project details:

Control Board Nucleo-F746ZG, Power Board X-Nucleo-IHM08M1, X-CUBE-MCSDK-FUL_5. Y. 1, st-stm32cubeide_1.6.1, stm32cubemx-win_v6-2-1, stm32cubef7_v1-16-1.

Errors:

1) unknown type name 'RTC_HandleTypeDef'(if LL)...

2) RTC_HandleTypeDef    hRTC_Handle; (if HAL)...

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Laurent Ca...
Lead II

Dear  @�?лек�?андр Микрюков​ 

Welcome to the STM32 Community

Where are coming from the source code you are trying to build?

Best regards

Laurent Ca...

АМикр.1
Associate

Good day.

The problem was solved by reinstalling Windows 10 x64 ...

But there was a new one: in the new Windows, the program Motor Pilot 5.Y.1 does not start... I tried with different versions of Microsoft Visual C++...

What could be the problem?

Sincerely, Alexander