cancel
Showing results for 
Search instead for 
Did you mean: 

How to configure MCSDK for multiple motors?

wJang.1
Associate II

Hello.

I have done position control of single motor using P-NUCLEO-IHM03 with GM2804 + AS5048a(pwm encoder). And I hope to control 3 motors for gimbal. So I'm planning to design a board using the MCU and motor driver which are used in the P-NUCLEO-IHM03

But, it seems that MCSDK does not support for multiple motor.

How can I set the basic IDE project for 3 motors?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
wJang.1
Associate II

I set IAR project for single motor control project using MotorControl Workbench 5.4.5

Laurent Ca...
Lead II

The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 SDK). 

Best regards

Laurent Ca...