User Activity

Hi!I am using STM32F746ZG + IHM08M1, I removed all bridges as recommended in Motor Profiler tool, and then I generated a project with Workbech. What I spotted that motor spins not that smooth like with F3 or F4 series. While testing I found that only...
Hi! I am using F746ZG + IHM08M1. And I need configuration with 2 insulated current sensors.My question is why in Workbench ICS gain is in range from -5V to 5V where the ADC max working range ist only 3.3V. Which current sensors should I buy 3.3V or 5...
Hi! I need to control a BLDC motor in FOC mode. I have a NUCLEO-H743ZI and IHM08M1, I know that they are not compatible with the ST morpho connector. But I decided to connect them manually with wires.On IHM08M1 board I removed capacitors C3, C5, C7, ...