STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4870 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9549 Views
  • 5 replies
  • 3 kudos

Resolved! Motor control SDK 5.1.0 and SW4STM32 not compiling

Posted on June 08, 2018 at 22:52Hi all,I'm trying to get started with the Motor Control SDK 5.1.0, after viewing the webinar. Hardware is a Nucleo F302R8, Nucleo-IHM07M1 (in 3 shunt configuration), and the bullrunning 1700 kV motor. The motor profil...

Resolved! steval-esc001v1 with sdk 5.1.1

Posted on July 10, 2018 at 15:36I find it a bit disappointing that there is no addon to sdk 5.1.1 for STEVAL-ESC001V1 and yet the board are still being sold. They are also being sold as RS485/UART/I2C/PWM platforms but the firmware does not handle I...

kyrreaa by Associate III
  • 1882 Views
  • 3 replies
  • 0 kudos

Errors in motor control library

Posted on July 11, 2018 at 11:21I use the SDK 4.3 and I have found this errors:- in open loop mode when enabled the V/F mode and reverse rotation the OL_Calc when increase the absolute speed, the voltage decreasevoid OL_Calc(COL this){  pVars_t pVar...