I used STSPIN32F0A as my motor control chip, the X_CUBE_MC workbench version is 5.4.4 , and the firmware package version is ST32 FW v1.11.2, then I generate the code ,but when I connect the MC workbench , I couldn't connect the MC workbench seria...
Hi Cristiana , in the following picture the Minimum start-up output speed suggest 15% maximum application speed ,while you suggest it should be close to the nominal motor speed, so I have no ideas.
Thank you. I have solved the question.This problem is caused by the hardware, I think the current sensing hardware forbidden the TIMER , so the communication lost.
Hi Cristiana. Thanks for your answer! I have checked the connection and the baudrate , they were ok. When I debugged the first time it could connect, but after changed the parameters of the current sensing , the serail communication was lost !
Hi Cristiana:I tried it according to your advices, but the problem remains. I think speed could not get into the closed loop system.I've tried a lot of other parameter settings,But it doesn't work too much, Do you have any other guidances that I ...