STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1729 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9574 Views
  • 5 replies
  • 3 kudos

Use STSW-SPIN3201 to drive PMSM motor

Posted on March 06, 2017 at 04:44Hello,I use STSW-SPIN3201 to drive a PMSM motor for industrial fan. After I modified the motor parameters by MC Workbench and re-builded the project. The motor can be driven. Now, I have one questions.The question is...

0690X00000606VdQAI.png 0690X00000606UaQAI.png

STEVAL-IHM042V1 connection failed

Posted on April 03, 2017 at 22:47Hello,                 I am using STEVAL-IHM042V1 and Motor Control Workbench. Everything was working fine until I tried to connect the board via the Motor Profiler.  STEVAL-IHM042V1 is not available for Motor Profi...

0690X00000606R3QAI.png

Over-current protection section

Posted on May 24, 2017 at 07:57Hello, All:I use (ST Motor control Workbench) parameters in power management where I set up some flow parameters, and then generate the file in Power stage, But  I did not find the parameters.h file to set my  paramete...

STEVAL-SPIN3201 randomly disconnects

Posted on May 26, 2017 at 16:09Working with STEVAL-SPIN3201. The board seems to randomly disconnect. It is not related to running a motor, just connected to motor control workbench. SPIN32F0 drive stays enumerated under windows. Anybody seen this?

USART not working in Motor Control Library

Posted on July 14, 2017 at 15:32I am using the Motor Control Library, to control a BLDC motor with Hall sensors. I would like to use the uart for my own purposes. If I enable uart, it dumps trash (since it tries to communicate with the MC workbench)...

About MotorProfiler motor data

Posted on July 18, 2017 at 05:36HiI'm working with the MotorProfiler to create the motor id data.But I create too much motor id data, so the motor control Workbench is a mess, as picture below.How can I delete some motor id data?Regards,Hank

0690X00000607IbQAI.png
Hank Wu by Associate
  • 872 Views
  • 1 replies
  • 0 kudos

LA052-080E3NL1 Shinano motor: how can I purchase it

Posted on July 28, 2017 at 14:43Hello,I would like to purchase 1 unit of LA052-080E3NL1 Shinano motor to be able to evaluate one of the reference project of the motor control workbench: How can I purchase it?Thank you.#motor #la052-080 #shinano #mot...

ST Motor Control Workbench: How to let the ''Enable differential term'' checkbox in ''Speed regulator'' be valid?

Posted on August 14, 2017 at 07:13I am using ST Motor Control Workbench and want to add differential term in the speed regulation of motor. But the checkbox 'Enable differential term' in 'Drive Management->Drive Settings->Speed Regulotor' is always ...

X TY by Associate
  • 1022 Views
  • 1 replies
  • 0 kudos

PFC doesn't work on STEVAL-IHM034V2 board

Posted on August 25, 2017 at 11:12Hi,i'm using the a STEVAL-IHM034V2 board for evaluation (PFC + FOC PMSM).I imported the project in ST Workbench 4.3. Generated files and compiled with IAR is OK. Then board is programmed.The motor starts but the PFC...