cancel
Showing results for 
Search instead for 
Did you mean: 

USART not working in Motor Control Library

Daniel Husztikd
Associate II
Posted on July 14, 2017 at 15:32

I am using the Motor Control Library, to control a BLDC motor with Hall sensors. I would like to use the uart for my own purposes. If I enable uart, it dumps trash (since it tries to communicate with the MC workbench) if I disable it, even if I configure it normally, it do not work. What do you suggest? Removing the MC Workbench communication part, or disabling the usart in the control_stage_parameters, and reconfigure again? 

Thanks!

Daniel

#foc #motor-control-workbench #stspin32f0 #motor
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards