STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1719 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4870 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9551 Views
  • 5 replies
  • 3 kudos

STM32F4 single shunt FOC

Hi,Using STM32F429VET trying to achieve FOC with single shunt resistor over 3phase bldc motor.I am using TIM1 and corresponding CC2, CC3, CC4 as PWM channels. CC1 is used to trigger ADC in regular mode reading current over shunt resistor in S1 and S2...

B-G431B-ESC1 FOC does not work correctly

Hi friends. Help me figure this out.Am I missing something, or is my board faulty? MCSDK 6.4.1Motor 12n14p  In 6-step mode, the motor operates correctly, and the phase signal waveform also appears normal.  But in FOC mode, something strange happens; ...

IMG20251030120600.jpg IMG20251030125934.jpg IMG20251030125524.jpg IMG20251030122801.jpg
ugomict by Associate
  • 416 Views
  • 2 replies
  • 1 kudos

EVSPIN32G4 Value Discrepancy

In Motor Control Workbench's Current Sensing tab.  It shows the default Shunt resistors at .005Ω.  The boards that were shipped to me have .01Ω.Is this by design?  What do I need to change in the Current Sensing tab to work properly with my hardware....

RinSxi by Associate
  • 299 Views
  • 1 replies
  • 0 kudos