2025-04-10 5:28 AM - edited 2025-04-10 5:29 AM
Hello,
I recorded plots using the real time scope of the MC Control Pilot, and I noticed that the generated file does not include all the points. There is a gap between 2 sample points and its recurring in every plot.
| TIMESTAMPS | I_Q_MEAS | I_D_MEAS | I_Q_REF | I_D_REF |
| 2209385 | 3.68703 | 0.129801 | 3.58856 | 0 |
| 2209386 | 3.62549 | 0.202535 | 3.58856 | 0 |
| 2209438 | 2.23236 | -0.421855 | 2.05668 | 0 |
| 2209439 | 2.24019 | -0.527039 | 2.26929 | 0 |
| 2209440 | 1.95821 | -0.649007 | 2.26929 | 0 |
There is at least 50 stamps which were lost.
What could be the issue?
I am on the latest MC Contol Pilot Version 1.2.12
Thank you
Solved! Go to Solution.
2025-04-10 5:46 AM
Sorry, I think I understood, I tried with 6 variables and it cannot hold it properly. I have a lot of missed samples. It works great with 4.
2025-04-10 5:46 AM
Sorry, I think I understood, I tried with 6 variables and it cannot hold it properly. I have a lot of missed samples. It works great with 4.