STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1764 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4916 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9646 Views
  • 5 replies
  • 3 kudos

X-NUCLEO IHM07M1 - Motor Profiler Problem

I bought a F401RE and an IHM07M1 to work on the subject BLDC a couple of weeks ago but, I could not profile the motor. My motor is T-Motor U8 170kw. It has 36 coils and 42 poles. I connected my boards successfully but, when I clicked "Start Profile" ...

0690X00000AqOy9QAF.jpg

Resolved! STM32G431CB Source code ?

Hy there,I would like to ask you, if there is possible to get the basic source code that you are uploading to the STM32G431CB ? I am using it with that basic code, with a MOTOR PROFILER GUI. I am trying to change the motor rotation periodicly (eg. af...

N_1 by Associate II
  • 4694 Views
  • 14 replies
  • 0 kudos

Unable to run high rpm bldc motor using Motor profiler

I have a Nucleo - F302R8 board with X-Nucleo - IHM07M1 BLDC motor driver. I'm trying to drive my bldc motor which is Emax rs 1106 - 6000kv using motor profiler software.Using the motor profiler software with suitable settings (pole pair = 6 , Max Spe...

HMoos by Associate
  • 1567 Views
  • 4 replies
  • 1 kudos

Motor Profiler doesn't work for Emax motors

Dear ST team,I have a Nucleo - F302R8 board with X-Nucleo - IHM07M1 BLDC motor driver. I'm trying to drive my bldc motor which is Emax rs 1106 - 6000kv using motor profiler software.Using the motor profiler software with suitable settings (pole pair ...

0690X000008ACYeQAO.png 0690X000008ACYZQA4.png
HMoos by Associate
  • 835 Views
  • 1 replies
  • 0 kudos

Delay when changing motor rotation?

Hy there,I would like to ask you, if there is possible to get the basic source code that you are uploading to the STM32G431CB ? I am using it with that basic code, with a MOTOR PROFILER GUI. I am trying to change the motor rotation periodicly (eg. af...

N_1 by Associate II
  • 989 Views
  • 1 replies
  • 0 kudos

ST Motor profiler with NUCLEO-F401

DearI am looking to test Nucleo-F401 with Motor driver IHM07-M1 but when stating motor profiler, this nucleo board does not appears in the list of supported board. When reading release not of Motor profiler, F401 should be in the supported board.Plea...

JEsca.1 by Associate II
  • 1481 Views
  • 3 replies
  • 0 kudos

I can't get the STM32G431RB to run the program to get the motor working. How do I get the motor to run smoothly?

I have set the jumper pins with respect to the user manual.The motor only runs after I profile it at the motor profiler, when I run the program into the board using the STM32CubeIDE, the motor stops running again. And when i want to profile it again ...

TYeo.1 by Associate
  • 909 Views
  • 1 replies
  • 0 kudos

How to configure IHM17M1 power board in ST Tools ?

I'm moving from the IHM07M1 power board to the IHM17M1. This uses the 5V STSPIN233 versus the L6230.None of the ST tools (Profiler, MCSDK, or MXCube) support this new board directly. Does anyone know the steps needed to configure the tools to use thi...

BTrem.1 by Senior II
  • 1298 Views
  • 2 replies
  • 0 kudos