STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1808 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4951 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9703 Views
  • 5 replies
  • 3 kudos

Motor Profiler doesn't work for Emax motors

Dear ST team,I have a Nucleo - F302R8 board with X-Nucleo - IHM07M1 BLDC motor driver. I'm trying to drive my bldc motor which is Emax rs 1106 - 6000kv using motor profiler software.Using the motor profiler software with suitable settings (pole pair ...

0690X000008ACYeQAO.png 0690X000008ACYZQA4.png
HMoos by Associate
  • 858 Views
  • 1 replies
  • 0 kudos

Delay when changing motor rotation?

Hy there,I would like to ask you, if there is possible to get the basic source code that you are uploading to the STM32G431CB ? I am using it with that basic code, with a MOTOR PROFILER GUI. I am trying to change the motor rotation periodicly (eg. af...

N_1 by Associate II
  • 1009 Views
  • 1 replies
  • 0 kudos

ST Motor profiler with NUCLEO-F401

DearI am looking to test Nucleo-F401 with Motor driver IHM07-M1 but when stating motor profiler, this nucleo board does not appears in the list of supported board. When reading release not of Motor profiler, F401 should be in the supported board.Plea...

JEsca.1 by Associate II
  • 1520 Views
  • 3 replies
  • 0 kudos

I can't get the STM32G431RB to run the program to get the motor working. How do I get the motor to run smoothly?

I have set the jumper pins with respect to the user manual.The motor only runs after I profile it at the motor profiler, when I run the program into the board using the STM32CubeIDE, the motor stops running again. And when i want to profile it again ...

TYeo.1 by Associate
  • 928 Views
  • 1 replies
  • 0 kudos

How to configure IHM17M1 power board in ST Tools ?

I'm moving from the IHM07M1 power board to the IHM17M1. This uses the 5V STSPIN233 versus the L6230.None of the ST tools (Profiler, MCSDK, or MXCube) support this new board directly. Does anyone know the steps needed to configure the tools to use thi...

BTrem.1 by Senior II
  • 1319 Views
  • 2 replies
  • 0 kudos

Motor Profiler fails every time. What am I doing wrong?

I bought a B-G431B-ESC1 to play with some BLDC motors salvaged from hard drives and optical drives. I'm supplying the board with 12V power, and have been able to get some erratic movement from the motors using the Monitor tool and one of the example ...

RTrev.1 by Associate II
  • 1016 Views
  • 1 replies
  • 0 kudos

B-G431B-ESC1 motor profiler outrunner BLDC not working

Hi,I tried using the motor profiler with B-G431B-ESC1 for an A2212/6T 2200kv motor but it just won't run. The profiler tries to move the motor and it sound's like it is trying to move, but never really rotates. After some time it says the profiler is...

DDomi.2 by Associate
  • 1195 Views
  • 1 replies
  • 0 kudos

Motor profiler fail in open loop test for my BLDC motor.

Hi!I am trying to profile the motor using B-G431B-ESC1 Discovery Kit.But the motor barely moves in the electrical model. The most successful one from my test was done without any values in Max Speed and Max Current. It ran up to 320, 2000, 1500, 1000...

Slee.3 by Associate II
  • 1090 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.