STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1731 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4876 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9575 Views
  • 5 replies
  • 3 kudos

EVSPIN32F06Q1S1 Questions?

Hello all.I am new to motor controllers and have some questions as I try to understand drivers for BLDCs.I am looking to drive a compressor (using BLDC motor driver).  I require up to 400V at about 2.5A (so 1000W max power).It seems that I could do t...

SWenn.1 by Senior III
  • 3035 Views
  • 4 replies
  • 0 kudos

doubt regarding STEVAL-SPIN3201

Still facing problem in STEVAL-SPIN3201. I  got errors like FOC  duration and software error. unable to start the motor. May i know what is the problem?I decreased PWM frequency, changed the execution rate, changed the PID values. Still the errors ar...

vishu by Associate II
  • 4354 Views
  • 3 replies
  • 0 kudos

Resolved! Motor spin without Motor Pilot program

Hello,I'm very biginner.By MCSDK6.2, I generated code and tried to spin 3 phases BLDC motor with code" MC_PrgramSpeedRampMotor1(1725, 2000);" and"MC_Startmotor1();"I inserted these code and built and tried to run, but it didn't work.The motor didn't ...

화면 캡처 2023-12-11 145920.jpg 화면 캡처 2023-12-11 145850.jpg
yourbryan by Associate II
  • 2726 Views
  • 3 replies
  • 0 kudos

Resolved! Servo buzzing and not working with STM32G030C8T6

Hi, I encountered a problem while trying to control servo motor(SG90) with my custom STM32G030C8T6 board. Servo is not moving at all and only buzzing quietly. I am supplying servo from 5V, board and servo have same GND. I checked servo power supply w...

MaciejG_0-1701631594463.png MaciejG_1-1701631675575.png MaciejG_2-1701631725500.png
MaciejG by Associate II
  • 3354 Views
  • 4 replies
  • 1 kudos

Resolved! B-G431B-ESC1 kit not working well

I've purchased a B-G431B-ESC1 kit and loaded it up with software (Details below)and soldered Phase, Power, and PWM/+5/Gnd wires.A couple problems and questions: -On most of my motors, there is no motion produced just some clicks, even though I've mat...

Problem with Motor profiler

[VERSION]: MCSDK 6.2.0 [TOOL]: Motor PROFILER v1.2.4EVALSTDRIVE101 + NUCLEO-F746ZG [DETAILS]: I have a sensorless project which work perfectly when the motor profiler option is disable. however, when the motor profiler option is enable, either the pr...

backb0ne by Associate II
  • 3991 Views
  • 5 replies
  • 0 kudos