STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Synopsis OTG_FS controller - how raw data are processed ?

Dear Community,I was trying to make composite USB2.0 device (FullSpeed) consisting of a UVC and HID component. Both the components I’ve tested before as a standalone device successfully. However after making a composite device accordingly to the HID-...

M G_2 by Associate III
  • 1831 Views
  • 2 replies
  • 0 kudos

2 Ethernet for STM32F427ZIT6

Hi,I am using STM32F427ZIT6 micro controller for one application.I want 2 ethernet interfaces for this project.Does STM32F427ZIT6 support 2 ethernets?Please help me how to achieve this.Thanks in advance,Dinesh

DKS by Associate II
  • 626 Views
  • 0 replies
  • 0 kudos

Usage of STM32f746G Ethernet to connect to the Cloud

Hello Guys,​I want to connect this board to AWS IoT Core using it's own Ethernet port onBoard. I'm struggling to understand how to use the Ethernet on the board.It's the first time I'm trying to connect a MCU to the Internet, and I feel a little lost...

CJava by Associate
  • 834 Views
  • 0 replies
  • 0 kudos

Trigger IAP ethernet mode from software

I'm running a NUCLEO-F429Zi discovery board inside a machine that I remotely control over the internet. I would like to do a firmware upgrade from remote as well.It can be done with TFTP in app programming, but most examples use a hardware button to ...

WSpar.1 by Associate III
  • 1086 Views
  • 1 replies
  • 0 kudos

STM32H7 ADC1 DMA Works while ADC3 DMA does nothing

So I have two channels configured basically with same settings. ADC1 works fine and DMA gets triggered and handled well. ADC3 DMA refuses to trigger any interrupt (not even an Error). The only difference is that ADC1 handles 14 channels while ADC3 ha...

Duddie by Associate II
  • 1878 Views
  • 3 replies
  • 0 kudos