STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CMSIS DSP arm_rfft_q15 troubleshooting

Hello I am trying to perform FFT on real data sampled with ADC However, first I need to perform it on test data that I generated inside my code to verify it would workI set parameters: frequency, buffer size, sampling rate (buffsize 512)then I gener...

hashtala by Associate II
  • 1764 Views
  • 0 replies
  • 0 kudos

f_open not working in stm32f4 with FATFS

I'm using STM32F4 Discovery board and its expansion board for SD-card interfacing. I'm using SD-cards with DMA2 and STM32CUBEIDE FW_F4 V1.24.2Before pointing out error I want to attach below link as a reference which I've used in my code -https://co...

0693W000002lhz4QAA.png
Rsrma.1 by Associate III
  • 1166 Views
  • 0 replies
  • 0 kudos

Resolved! Custom Bootloader STM32H750

Hello,I am developing a simple GUI for a custom board based STM32H750 MCU.My requirements are the following:Both application code/data and touchGFX images/fonts are stored in and external QSPI (0x90000000) The entire application must be executed in t...

PLago.2 by Associate II
  • 1844 Views
  • 1 replies
  • 0 kudos

Connect to MQTT Broker with STM32F746G Discovery

Hi, I'm trying to connect to my MQTT Broker with STM32F7 Discovery kit.Firstly, I used MQTT Client in LwIP stack. When I call this function: mqtt_client_connect()the Error return ERR_RTE, mean Routing Error /** Routing problem.     */ ERR_RTE    = -4...

Resolved! STM32F4xx and STM32H7xx CUBE HAL SPI BUGS

High Level Problem Description:STM32F4xx: Produced on STM32F427IIHxWhat happens:When SPI as master, full duplex, 8 bit & ~1MHz clock speed and doing longer transmissions (e.g. 10 - 60 bytes) using interrupts the current implementation in Keil::STM32F...