STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F7508 MCU freeze

Hello all,I have an STM32F7508-Discovery board (STM32F750N8H6 MCU) with a custom UI application on top, using LTDC and DMA2D in interrupt mode, and continuously filling the full display with red/blue. The Stm32CubeF7 v1.16.0 is used as an SDK.With th...

VVasi.1 by Associate II
  • 4371 Views
  • 6 replies
  • 0 kudos

How to connect the STM32F407 discovery and the USB3300

Dear Community,as I read from other posts e.g. here: https://community.st.com/s/question/0D50X00009XkhBISAZ/stm32f4-discovery-usb3300-ulpi-phyit is possible that the STM32f407 discovery board can be successfully connected via ULPI interface to a USB3...

M G_2 by Associate III
  • 3324 Views
  • 2 replies
  • 0 kudos

Report descriptor for keyboard

I want to know how to set report descriptor for keyboard which is going to send 16 byte of data to PC.I am trying to set default keyboard descriptor as below.... __ALIGN_BEGIN static uint8_t HID_MOUSE_ReportDesc[HID_MOUSE_REPORT_DESC_SIZE] __ALIGN_E...

Bs.1 by Associate II
  • 989 Views
  • 0 replies
  • 0 kudos

Cannot see USB_FS on STM32F373VCT6 as VCP.

Hi I have STM32F373VCT6 on the board that I am bringing up. I am trying to open up the USB_FS as VCP. I use 20 MHz oscillator, which gives 48 Mhz USB clock and 24 MHz for APB2. I use the code below: while (1) {  /* USER CODE END WHILE */  /* USER CO...

BPart.1 by Associate II
  • 719 Views
  • 0 replies
  • 0 kudos

How to send 16 bytes of data from USB keyboard(Using HID class ) to PC.I have sent 8 byte data it working properly. Unable to send 16 byte data.

I have done setting in Report descriptor as below, 0x05, 0x01,          // USAGE_PAGE (Generic Desktop)   0x09, 0x06,          // USAGE (Keyboard)   0xa1, 0x01,          // COLLECTION (Application)   0x75, 0x01,          //  REPORT_SIZE (1)   0x95, 0...

Bs.1 by Associate II
  • 832 Views
  • 0 replies
  • 0 kudos

Resolved! usbd_dfu_if.c

Hi, I'm trying to implement my own DFU bootloader interface, since I'm using a custom STM32F446RET board.Been looking into STM32F446ZE-Nucleo DFU_Standalone project to get some ideas, but seems to be quite different to my new custom CubeMX created pr...

VictorPr by Associate II
  • 1608 Views
  • 1 replies
  • 0 kudos

Is UM1884 (STM32L4/L4+ HAL and low-layer drivers UM) description for RCC_PLLInitTypeDef inconsistent with header file 'stm32l4xx_hal_rcc.h' generated by STM32CUBEMX with respect to PLLP, PLLR parameter definitions?

The structure definition for RCC_PLLInitTypeDef in the header file 'stm32l4xx_hal_rcc.h', generated by STM32CUBEMX, is inconsistent with the RCC_PLLInitTypeDef struct description in the STM32L4/L4+ HAL and low-layer drivers UM (UM1884 Rev8) page 821,...

Tritc.1 by Associate
  • 1769 Views
  • 1 replies
  • 0 kudos