STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MCU serial number

For some reasons it will be good to write my own MCU serial number for USB purpose.. Is it possible to change seria number of hte MCU and how to do this...

MJova.1 by Associate II
  • 2805 Views
  • 9 replies
  • 0 kudos

Resolved! FOTA in STM32L0

For an application, I need to implement FOTA through UART/USB for STM32L0 microcontroller. Are there any examples or firmware packages available for this?

ASiva.1 by Associate III
  • 1143 Views
  • 1 replies
  • 0 kudos

Resolved! Error with timeouts constants in stm32f7xx_hal_sd.c in SD_SendSDStatus and SD_FindSCR cause indefinite hangs.

Both these functions contain the code:"if((HAL_GetTick() - tickstart) >= SDMMC_DATATIMEOUT)"However SDMMC_DATATIMEOUT is defined as 0xFFFFFFFF so the timeout is very long (49 days with a 1ms tick) and therefore never occurs.That upshot is that if the...

SGars by Associate II
  • 3592 Views
  • 5 replies
  • 0 kudos

STM32L4 usb bug

Hello, I am using the STM32L4 Micro-chip on a board I am using, and I can across a weird issue with the usb. When ever I was running iar and trying to open up the com port within another serial program, the serial program was unable to open the com p...

DAgui.3 by Associate
  • 698 Views
  • 0 replies
  • 0 kudos

Resolved! stm32h723 lwip configuration problem

I wanted to replace my system that used to work with stm32f407VGT6 with STM32H723VET6 as it is cheaper.I designed a new pcb, followed the steps in the link below and created a project.https://community.st.com/s/article/How-to-create-project-for-STM32...

STM32F4 HAL RTC Library Output

It appears that if the output bit is set (RTC_CR_COE) it doesn't get cleared when the RTC is initialized.In the library code:HAL_StatusTypeDef HAL_RTC_Init(RTC_HandleTypeDef *hrtc){... else {   /* Clear RTC_CR FMT, OSEL and POL Bits */   hrtc->Instan...

KKobe.1 by Associate
  • 1392 Views
  • 2 replies
  • 0 kudos

STM32F0 USB Audio Record

Is there any working example to do USB Audio Recording using the STM32F0? I need to send audio received by the I2S port on the STM32F0 and send it out to the host PC via USB. I have seen AN4711 and also have the Record working on the F7 with the hel...

EThur.1 by Associate
  • 969 Views
  • 0 replies
  • 0 kudos