cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Choice for USB-PD STM32F0 + STUSB1602

Leo Tai
Associate II

Hi,

I currently working on a USB PD project. I am quite interested in ST solution. I need a DRP, dual power role, features so STUSB1602 should be included in the design. I just found the application firmware is developed based on STM32F071RB and the system is running in FreeRTOS. I can modify the application firmware in the nucleo demo board.

I would like to choose a smaller MCU which is compatible to the STM32F071RB. I targeted the STM32F071CB 48 pins UFQFPN.

My question is can I directly flash the STM32F071RB firmware to STM32F071CB?

Thank you very much

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0