STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to flash the compiled code to stm32l431cb

Hi Experts,I am planning to use stm32l431cb - as it is sufficient controller with 48 pin for my use case. Basically I am trying to find out, how to flash my code into stm32l431cb controller.I referred to a. https://www.st.com/resource/en/datasheet/st...

PD S.1 by Associate II
  • 2898 Views
  • 6 replies
  • 0 kudos

Entering into system Bootloader mode with IWDG?

Good electronical morning to everyone.Context:I find myself needing to enter stm32´s system bootloader during runtime on command.I asigned a GPIO with a simple RC circuit to pull the BOOT0 pin high.The system reset is done by IWDG exception, i just s...

0693W000008GH1FQAW.png
Javier1 by Principal
  • 2506 Views
  • 2 replies
  • 1 kudos

ICMP-IPv4 total length exceeds packet length

I have a problem with +500byte ICMP packet, I am using ubuntu 16.04 and firewall inactive. When I try to send ping with this command ping -s 500 192.168.1.127 ping is successfull, but when I try to send this ping -s 580 192.168.1.8 ping reply didnt a...

DCtech by Associate II
  • 1613 Views
  • 0 replies
  • 0 kudos

STM32f769II USB_OTG_FS Non periodic TX_FIFO problem

Background of a problem:I am using ST low level libraries for USB OTG and USB HOST. I wrote my own USB class for ASIX USB-ETH adapter based on template and CDC class. The problem was that solution presented by ST driver was to slow. I could only send...

BSzef.1 by Associate
  • 1133 Views
  • 1 replies
  • 0 kudos

Hello, i am implementing a HAL CAN Driver for my STM32F405. I am using a TJA1048 as a Tranciever. Down below there is my Source Code. If i want to Transmit one Message, it ends in the Errorcode: HAL_CAN_ERROR_TX_TERR0. So do you know whats wrong ?

My APB1 Clock Frequency is 42Mhz.Init:hcan1.Instance = CAN1; hcan1.Init.TimeTriggeredMode = DISABLE; hcan1.Init.AutoBusOff = ENABLE; hcan1.Init.AutoWakeUp = DISABLE; hcan1.Init.AutoRetransmission = DISABLE; hcan1.Init.ReceiveFifoLocked = DISABLE; hca...

SLeit.1 by Associate
  • 1697 Views
  • 1 replies
  • 0 kudos

PDM 2 PCM DMA buffer size confusion

Hello,I have a PDM MEMS microphone that I am reading in I2S master receive mode. I am trying to take this data and put it in a FIFO buffer and then output the data over UART using DMA. I must be confusing the buffer sizes because I get mostly zeros...

kcire L. by Associate III
  • 865 Views
  • 0 replies
  • 0 kudos