cancel
Showing results for 
Search instead for 
Did you mean: 

Am using Windows 7 Ultimate , x86. Also tried a separate Linux Ubuntu 18.04.3 PC , with same result. Can't get Virtual COM Port to enumerate using STSW-STM32102 USB driver installation package. Get, "device descriptor read/64, error -71" reported.

MHodg.1406
Associate

Does anyone know how to edit the device descriptor when using this driver package and can explain this in detail ? The uC is a STM32L082KZT6. The Virtual COM Port (VID 0483 PID 5740) is a USB CDC class 2 device. The associated USB DFU (VID 0483 PID DF11) device enumerates OK, every time. Posted on this issue twice previously, hopefully, third time lucky, all help appreciated!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0