STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 code missing

Hi Colleagues: Our new product use STM32F407 to realize the function of TCP/IP with RJ45. The problem is the device will error when 10 days later.The bad device restart every four seconds and We must download again.Please help us to solve the pr...

LwIP (PPP) not work with X-CUBE-CELLULAR

Hello,​I am evaluating PPP with X-CUBE-CELLULAR but it doesn't work on my board.​Test environmentSMT32 CubeIDE 1.6.0Customized board (STM32L4A6VG) with the Quectel BG96 on UART interface (no flow control)X-CUBE-CELLULAR V5.2Purpose:Using BG96 with PP...

SL61 by Associate II
  • 4672 Views
  • 4 replies
  • 0 kudos

Systick and FreeRTOS Question

My client has an application which uses FreeRTOS. Recently I wanted to do a small, simple test. I wrote a couple dozen lines of code and put it in main() before the FreeRTOS scheduler starts (my test code ends in a while(1) loop, to FreeRTOS never ge...

USB HOST MSC: Function f_findfirst() returns FR_DISK_ERR error despite USB Stick has been successfully mounted

I am trying to implement simple appication to scan existing files in USB stick in root directory. I just use ST sample as reference and following is the user call back code. The error is line 27It manage to reach :Appli_state = APPLICATION_START; and...

BParh.1 by Senior III
  • 1027 Views
  • 1 replies
  • 0 kudos

DHCP not detecting in my STM32f4 Disco Board while interfacing DP83848 MAU board. I performed LWIP with RTOS, DHCP enabled but does not works.

DHCP not detecting in my STM32f4 Disco Board while interfacing DP83848 MAU board. I performed LWIP with RTOS, DHCP enabled but does not works.Auto-Negotiation Enabled, MII interfacing, Phy Address 01. All pins are correctly connected same as STM32CUB...

SVerm.3 by Associate III
  • 826 Views
  • 0 replies
  • 0 kudos