Skip to main content
TMark.14
Associate III
June 24, 2020
Question

STM32F303VC eval board - usb is not recognized

  • June 24, 2020
  • 0 replies
  • 457 views

I use Atollic IDE v9.3.0 and Segger J-Link J-Trace Pro and built in STlink sometimes.

Using the STM32cube mx v5.6.1 I generated projects for USB CDC class with STM32303E- EVAL and NUCLEO-F303RE, neither board is recognized by the USB host (PC with Win10).

Using STM32303E- EVAL, I configure PB8 (USB Disconnect) as Output Low by default.

I found the USB library STM32_USB-FS-Device_Lib_V4.1.0, there is a project Virtual_COM_Port and running this project the usb is recognized by the host and it shows that STM Virtual Com port is connected.

While debugging cube mx generated project I see that the USB->CNTR register has set  FSUSP: Force suspend bit which is not set if I am debugging project from the STM32_USB-FS-Device_Lib_V4.1.0 library.

Also for some reason the USBD_StatusTypeDef USBD_Start(USBD_HandleTypeDef *pdev) function from the usbd_core.c file is empty.

Can someone tell me what I can do to make the USB CDC working on stm32f303?

This topic has been closed for replies.