2020-06-23 12:00 PM
Hello !
I am trying to make 1 STM32 that handles 2 HIDs, one keyboard (HID_MOUSE_ReportDescK[HID_MOUSE_REPORT_DESC_SIZEK]), one mouse (HID_MOUSE_ReportDesc[HID_MOUSE_REPORT_DESC_SIZE]).
I use a STM32F103C8T6.
I tried to create 2 int (used as boolean) that permit to know if it has to be a keyboard or a mouse.
Those int are also used like that:
#if mouseEnabled == 1
HID_MOUSE_REPORT_DESC_SIZE
#elif keyboardEnabled == 1
HID_MOUSE_REPORT_DESC_SIZEK,
#endif if (req->wValue >> 8 == HID_REPORT_DESC && mouseEnabled == 1)
{
len = MIN(HID_MOUSE_REPORT_DESC_SIZE, req->wLength);
pbuf = HID_MOUSE_ReportDesc;
}
else if (req->wValue >> 8 == HID_REPORT_DESC && keyboardEnabled == 1)
{
len = MIN(HID_MOUSE_REPORT_DESC_SIZEK, req->wLength);
pbuf = HID_MOUSE_ReportDescK;
}But, I am a beginner in the MCUs / programming world it's why I figured lately that what I made, works only when I change the int before debugging. I also tried many other things that came to fail.
Thank you for your help.
2020-06-23 3:40 PM
Modify the HID example so that it creates two separate USBH_ClassTypeDef objects,
assign each to the two host controllers:
USBH_ClassTypeDef hidClass1, hidClass2 ;
// Initialize these with HID class ...
.........
USBH_RegisterClass(&hUsbHostHS, hidClass1);
USBH_RegisterClass(&hUsbHostFS, hidClass2);
So each host controller has its own "class" object.
This way you can connect two HID devices to STM32.
-- pa
2020-06-23 5:26 PM
I maybe was unclear about that, but I don't want two HID devices. I would like to create a keyboard with a STM32 that can make also mouse tools (ex: traditional keyboard, though, up arrow increase the mouse cursor y axis.
About my main.c file, I initialize
extern USBD_HandleTypeDef hUsbDeviceFS;
uint8_t HID_buffer[8] = { 0 };For the buttons part
if (HAL_GPIO_ReadPin( GPIOA, GPIO_PIN_15) == GPIO_PIN_SET) // keyboard button
{
// keyboardEnabled = 1;
HID_buffer[2] = 10;
USBD_HID_SendReport(&hUsbDeviceFS, HID_buffer, 8);
}
else{
// keyboardEnabled = 0;
HID_buffer[2] = 0;
USBD_HID_SendReport(&hUsbDeviceFS, HID_buffer, 8);
}
if (HAL_GPIO_ReadPin( GPIOB, GPIO_PIN_5) == GPIO_PIN_SET) //mouse button
{
// mouseEnabled = 1;
HID_buffer[3] = 10;
USBD_HID_SendReport(&hUsbDeviceFS, HID_buffer, 8);
}
else{
// mouseEnabled = 0;
HID_buffer[3] = 0;
USBD_HID_SendReport(&hUsbDeviceFS, HID_buffer, 8);
}I also use the HID class in STM32CubeIDE, not customHID one, maybe this is important to know.
Thank you some much for helping me.