STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32l431 SWD only connects at 5 kHz

I have a board with an stm32l431rc. I have some sample code generated by CubeMX, and it boots up just fine.I'm trying to work with zephyr v2.5.0. Zephyr has hal and pinctrl dtsi files for this MCU, so adding a new board was pretty straightforward.I s...

CVita.1 by Associate
  • 1693 Views
  • 2 replies
  • 0 kudos

USB read/write permission

Hello,Please find the Product details below:NUCLEO-H743ZI2I have purchased the above board for developing application to interface with the Lan9253 device.I have installed the device drivers downloaded from the STMicroelectronics site.Do I need any U...

Ntall.1 by Associate II
  • 2348 Views
  • 6 replies
  • 0 kudos

Resolved! Where can we find LwIP example code?

In this document:https://www.st.com/resource/en/user_manual/dm00103685-developing-applications-on-stm32cube-with-lwip-tcpip-stack-stmicroelectronics.pdfThey talk about some examples. Where can I find the example code source?

Jvan .10 by Associate III
  • 1037 Views
  • 1 replies
  • 0 kudos

Resolved! Transmit multiple data using UART & FREE RTOS

Hi,Iam using STM32 NUCLEO F401RE BOARD to send multiple data to PC using UART Printf.I have created different tasks(4 tasks) for different computations and finally one dedicated task to send all the data computed to be sent via UART using Printf.for...

SMour.2 by Associate III
  • 5195 Views
  • 8 replies
  • 0 kudos

Resolved! Where to find B-L462E-CELL1 examples?

Hi, I recently got a B-L462E-CELL1 discovery board and am eager to start some projects with cellular connectivity. But I really don't know where to start and was planning to learn a lot from the examples that where promised when I read about the devi...

RBrat.1 by Associate
  • 1075 Views
  • 2 replies
  • 0 kudos

Running LwIP resulting in a HardFault

I've generated the LwIP code with CubeMX for my Nucleo H745ZI-Q and used this guide to make extra settings:https://github.com/AnielShri/STM32H745_EthernetNow when I run my program, it results in a HardFault. I've attached the memory .ld files, anyone...

0693W00000AO4tIQAT.png 0693W00000AO4tXQAT.png 0693W00000AO4tmQAD.png 0693W00000AO4qtQAD.png
Jvan .10 by Associate III
  • 1915 Views
  • 1 replies
  • 0 kudos

Is NTFS possible on STM32

Hey everyone,I'll just wanted to ask, if its possible to read a USB Stick with NTFS Filesystem and ext4 on STM32. I'm only finding information about FatFS.I've also read, that NTFS is licensed so if that is not possible on STM32: Is there any workaro...

FLow.1 by Associate
  • 3386 Views
  • 3 replies
  • 0 kudos