STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 USB polling: Which interrupt line?

Hi. I'm having trouble managing a USB slave on STM32L4 using interrupt. I'm able to make it work using polling, and on a previous F3 project, had polling working.From RM, NVIC section, F3 has 3 USB lines: Wakeup, LP, and HP (HP and LP are shared with...

DOCon.1 by Senior
  • 2421 Views
  • 5 replies
  • 0 kudos

Resolved! ETH DMAMR SWR always set, why?

Hello , I have STM32H750x MCU. I would like to know why the ETH DMAMR->SWR (software reset bit) is still ALWAYS SET?I know even the HAL driver is trying to do the SW reset on the ETH DMA and MAC. I know I should have an enabled and stable clock for t...

Peter_TEC by Associate II
  • 5447 Views
  • 7 replies
  • 0 kudos

Resolved! STM32CubeMx I2C_TwoBoards_ComDMA Issue

In the example while(HAL_I2C_Master_Transmit_DMA(&I2cHandle, (uint16_t)I2C_ADDRESS, (uint8_t*)aTxBuffer, TXBUFFERSIZE)!= HAL_OK) { /* Error_Handler() function is called when Timeout error occurs. When Acknowledge failure occurs (Slave d...

Iirel.1 by Associate
  • 1317 Views
  • 1 replies
  • 0 kudos

Question on 'pulse' section is stm32Cube

hello everyone, I am trying to generate a square wave at a desired frequency. I am supposed to use the TIM3 peripheral. I selected the "Output compare CH1" for channel 1 section and under this section it asks me for a pulse value (which I know is th...

GSant.5 by Associate II
  • 1677 Views
  • 3 replies
  • 0 kudos

STM32H750 HAL_SPI driver function HAL_SPI_TransmitReceive(......) is called in my EXTI9_5_IRQHandler() interrupt function , It runs dead loop, and can't return.

If the H7 HAL_SPI driver function HAL_SPI_TransmitReceive(......) is called in my main(),It runs correctly, I can transmit and receive data correctly. But it is called in my EXTI9_5_IRQHandler() interrupt , It runs dead loop, and can't return.

ZMinZ.1 by Associate
  • 1077 Views
  • 1 replies
  • 0 kudos

Resolved! Bootloader Versions of STM32F42xxx/43xxx

Hello all,I have STM32F439 MCU.I use STM32CubeProgrammer to program the MCU through ST Bootloader.STM32CubeProgrammer writes:Bootloader protocol version: 3.1According to AN2606 (STM32 microcontroller system memory boot mode) the valid version for ST...

HAL_RCC_OscConfig ends in HardFault_Handler

HiI'm using a Nucleo-144 with a STM32F767ZI.I have included in my project FreeRTOS and FreeRTOS-IP although that may not be related with the problem, since the crash happens before reaching the initialisation of FreeRTOS.My problem seems to be that H...

EGonc.2 by Associate II
  • 1310 Views
  • 1 replies
  • 0 kudos