STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! NUCLEO-L4R5ZI Changing timebase source fails

Hello,STM32Cube FW_L4 V1.17.0When changing the timebase of the systick, the HAL_Init() function no longer returns and it goes off to system memory in a loop.To replicate, start a new project with for the NUCLEO-L4R5ZI, initialise all pins to the defa...

DM.7 by Associate III
  • 1462 Views
  • 2 replies
  • 0 kudos

Resolved! Default bootloader source code?

My dedicated hardware does not support uart/i2c/spi on the pins that are mentioned in AN2606. To update firmware IAP, I need to write my own bootloader that behaves the same as the default one (I want to use stm32flash tool as host, which fasten my w...

BMich.2 by Associate
  • 1453 Views
  • 2 replies
  • 0 kudos

Fatfs f_mount and f_getfree

I am using NUCLEO H743ZI2 with Fatfs and FreeRTOS V2. The program is working now, but I have one issue on free size of SD card. After I use f_mount to mount my SD Card, In structure FATFS variables, last cluster and free cluster are not correct. If ...

yang hong by Associate III
  • 1790 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L562 SD card HAL_SD_ERROR_DATA_CRC_FAIL

I'm trying to run FAT over SD MMC. But it does not work in SD initial stage... I'm using CubeMX.The simplest one code: status = HAL_SD_Init(&hsd1); if(status != HAL_OK) { debug_print_message("---SD card initialize failed!\n"); HAL_Del...

0693W00000D2cwEQAR.png
SLesh.1 by Associate III
  • 2457 Views
  • 3 replies
  • 0 kudos

Resolved! DFSDM with DMA doesn't give expected results

Hello,I am working on application that would use microphone array. Together with STM32H735IG board I decided to use STEVAL-MIC001V1 microphone array connected via DFSDM interface. I based my project on example available in CubeMX - DFSDM_AudioRecord ...

PZare.1 by Associate II
  • 2315 Views
  • 1 replies
  • 0 kudos

STM32F103 USB cdc receiver is very slow

i am using stm32f103 for one project. Previously we were using UART interface to transfer data but now we want to use USB CDC interface for the same.i configured the usb in cdc mode and it is working also. I am facing one issue like data receiving is...

SS.Sagar by Associate III
  • 2330 Views
  • 3 replies
  • 0 kudos