Hi,
I am using STM32l4R9 and using uCosIII Os with 16MHz CPU frequency. The project works fine with bare metal but getting failed when creating micrium tasks. The same micrium project works fine with 48MHz CPU frequency.
TIA!
Hi,I am using STM32L4R9 USB along with STUSB1600 in device mode only. I get the device connect interrupt USBD_LL_DevConnected when USB host is connected either DM DP lines are connected or not. I need to detect if connection and enumeration on USB ho...
Hello, I am trying to use STL for STM32L4R5ZIT6, while the example project given on STM32L476G. What are the modifications needed to use this example code for STM32L4R5ZI? Referred document: AN4435Thanks in advance!