STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FatFs + SDMMC + DATAEND interrupt

I've been struggling to get FatFs working on STM32L496 / L471 for some time now. At present my code uses polling which even at low card clock with certain interrupts disabled is not reliable enough, giving me random FR_DISK_ERR. I know I have to get ...

MPage.1 by Associate II
  • 1826 Views
  • 1 replies
  • 0 kudos

Resolved! Is there any USBX Host Class - Audio/Video example?

I'd like to develop USB host application with Audio and/or Video class.Is there any working example project or code snippet?I checked STM32 HCD driver file - -ux_hcd_stam32_periodic_schedule.c, but it always generates EP_TYPE_INTR packet. How can I s...

sirius506 by Associate III
  • 2271 Views
  • 4 replies
  • 0 kudos

Coupon not valid

Hello, when I try to order the NUCLEO-H723ZG and place the coupon I get this message "The coupon code "WS-H723ZG-1ZGI-EMEA-2021" is not valid." I tryed several times in the last weeks but no way out.Thanks in adavance

MRoss.7 by Associate
  • 887 Views
  • 1 replies
  • 0 kudos

Hard Fault after receiving packet with LwIP

Thank you for helping.The microcomputer is STM32F769I.I wrote the code with reference to the HttpServer sample.TCP / IP server application.When I send a packet from a TCP client, I can receive it, but then it HardFaults.It seems to happen after relea...

Ebun.1 by Senior
  • 1945 Views
  • 2 replies
  • 0 kudos

Edge computing IoT Device for Voice processing

I would like to build edge computing IoT Device for voice commands recognition. (In short Speech Recognition at edge). What is best suitable STM32 device with digital microphone and speaker interface (similar to echodot or google home, where processi...

YSN by Senior
  • 1813 Views
  • 1 replies
  • 0 kudos

Use of USB FS I want to Design Application

Hi!With the use of USB FS I want to design application & emwin on board stm32h743i-eval. When usb is attached, the function of enumeration does not work. Function USBH_Get_DevDesc get back as USBH_BUSY always and USB is found in condition of ENUM_IDL...

by Not applicable
  • 1044 Views
  • 2 replies
  • 0 kudos

Unable to order free NUCLEO-H723ZG board

Hello I've received an email to "Order your free board for the workshop STM32Cube with Azure RTOS".But I haven't received any email with the coupon. I've check my email, the trash folder and the spam folder.

AGuzzi by Associate
  • 1150 Views
  • 2 replies
  • 0 kudos