STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Nucleo-F303RE USB HID Not working

I'm prototyping a project, and im struggling to get USB HID working on the Nucleo F303RE board. I've connected an external micro-usb breakout board to the nucleo via the PA12 & PA11 pins as configured in the CubeIDE. However running the most basic us...

STM32H7 Reading DMA Context Descriptor

Hello There!I have some questions regarding the STM32h747 and DMA Descriptors.Our ultimate goal is to read the Timestamps captured by the MAC. In the Reference Manual (page 2995) it says that the timestamp will be returned in the RDES0/1 fields of th...

TSieg.1 by Associate
  • 1138 Views
  • 0 replies
  • 0 kudos

Resolved! How can I communicate with my HOST MCU via USB with a Device MCU, if the device only uses an FTDI chip?

My Partner has an hardware, which only communicate over USB (FTDI) with other hardware platforms. At the moment there is no possibilty to change the hardware.Unfortunately I have to write the USB Host with my STM32H7A3ZI. My first steps was to use th...

RRuoc.1 by Associate II
  • 3067 Views
  • 5 replies
  • 0 kudos

Resolved! Bug in CubeMX with STM32H747 DualCore and AzureRTOS

Hello, maybe I found a bug in CubeMX.Actually it is not possible for me to generate Code for the DualCore derivates to get AzureRTOS active on BOTH cores.After activating a new project with AzureRTOS selected for both cores, all of the port-*.c and *...

AZorn.1 by Associate III
  • 2131 Views
  • 8 replies
  • 0 kudos

STM32H747I-DISCO-CM7 SAI audio interface DMA problem

Hello there,I am trying to build a custom voice AI solution using STM32H747I-DISCO development kit, for which I generated the NN library code by importing a .tflite model via STM32CubeIDE and it works fine with a static Input buffer.Now, I am trying ...

BPraj.1 by Associate II
  • 1868 Views
  • 2 replies
  • 0 kudos

Resolved! How to increase incoming packet size for LWIP?

Hello,I just started with implementing LWIP in the NUCLEO H753ZI. I got the UDP server working and receiving incoming UDP data and echo back to the client. However, if the client sends anything greater than 16 bytes, my board runs into memory error a...

0693W00000GXW61QAH.png 0693W00000GXW5mQAH.png 0693W00000GXW5cQAH.png 0693W00000GXW29QAH.png
ANguy.5 by Associate II
  • 1658 Views
  • 1 replies
  • 0 kudos

Resolved! tx_thread_sleep Hard Fault

HelloI am creating a project via STM32CubeIDE (V1.7.0) for a STM32F411 discovery including AzureRTOS.When I include in my thread a call to tx_thread_sleep the program stops in HardFault_Handler when this function is called.I have checked threads are ...

MR7 by Associate II
  • 2698 Views
  • 2 replies
  • 0 kudos

RNDIS demo project with FreeRTOS+TCP

Hello community!To whom it may interest:I made a RNDIS demo project and would like to share it with you.It is using HAL with my rndis library and FreeRTOS on top. Further I have implemented a lightweight http server, dns and dhcp server. The demo wor...

NKorn.12 by Associate II
  • 1948 Views
  • 0 replies
  • 3 kudos