STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

how to sync a uart dma receive for gps parsing

Hi, I'm working with a stm32f722 and a ublox f9p gps. I just have 2 ubx messages. One with 36 bytes long and the other with 72 bytes. They income with a variable interval between them (a couple of byte time at most, usually they come together). This ...

Lgarb.1 by Associate II
  • 6319 Views
  • 8 replies
  • 0 kudos

Resolved! Azure RTOS USBX device descriptor errors

I'm trying to recreate one of the example projects from https://github.com/STMicroelectronics/x-cube-azrtos-f4/tree/main/Projects/STM32469I-Discovery/Applications/USBX/Ux_Device_CDC_ACM I have a nucleo-F446ZE board for this test. I created the bare p...

jbramble by Associate II
  • 3885 Views
  • 5 replies
  • 0 kudos

Resolved! Update Schedule of HAL_Eth

Hi, is it possible to get a round-about info on the expected Hal-Eth update?In the release notes of the Hal-Driver it is flagged as "A full rework of the ETH HAL driver is planned.." , but the last release has been in February. I would like to avoid ...

JRS by Associate III
  • 1890 Views
  • 3 replies
  • 2 kudos

Resolved! How can I handle "SD card is being extracted and reinserted while system is running" (STM32H7 with FATFS)?

I am stuggling with following task:My system is running with SDCard perfectly when either SD card is inserted or not at power on. So file system is working if card is present at power on.It also detects when the card is extracted while system is runn...

GS1 by Senior III
  • 1562 Views
  • 1 replies
  • 0 kudos

Resolved! [bug fixes] STM32H7 Ethernet

@Amel NASRI​, @ranran​, @Piranha​, @Harrold​, @Pavel A.​ V2 of my fixes and improvements to H7_FW V1.5.0/V1.6.0 Ethernet...Changes includeDecoupling receive buffers from receive descriptors so buffers may be held any length time without choking recei...

alister by Lead
  • 65127 Views
  • 97 replies
  • 14 kudos