STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743 with USB HS, FUSB2805 not detected

I have a custom board with STM32H743VIT6 connected to an external USB HS PHY, the FUSB2805MLX.I am trying to run a bare minimum example setup in STM32CubeMx. Just including a USB HS connection and the device in USB VCP mode. The pin setup is correct,...

LFjær.1 by Associate
  • 1774 Views
  • 1 replies
  • 0 kudos

USART HAL Compatibility with FreeRTOS

I'm trying to send data over the Virtual COM Port of an STM32H745I dev board to a Termite shell inside a FreeRTOS task. I setup USART 3 to run at the settings matching the documentation's virtual COM Port settings, and call the generated initializati...

0693W00000LvUjYQAV.png
EMurp.1 by Associate II
  • 1782 Views
  • 2 replies
  • 0 kudos

STM32L433 IAP

Hi,I have 2 partitions on the STM32L433cct6 :IAP (to upgrade via USB) : 0x08000000 - 0x0800C000Application : 0x0800C000 - 0x08040000I have a function to jump to the application :/* Jump to user application */ JumpAddress = *(__...

MMerc.1 by Senior
  • 2414 Views
  • 4 replies
  • 0 kudos

STM32L0 ADC two channel polling

Posted on November 06, 2016 at 21:04Hi, I am coding an application for STM32L053R8 using the HAL functions. Right now I need to read continuously two analog values via ADC. Because there is no need of high frequency readings, I want to try doing it ...

STM32L0 - How to set Single-Ended Mode on an ADC Channel on STM32 using the HAL library?

Current settings seem to only produce 0x000 to 0x7FF . The HAL API on the STM32L0 only has 2 Parameters in the ADC ChannelConf Type:typedef struct{ uint32_t Channel;    uint32_t Rank;         }ADC_ChannelConfTypeDef;Which is Clearly missing the : ...

X-CUBE-USB-PD install

Hello. I'm trying to figure out X-CUBE-USB-PD. As I understand it, this is an extension for CubeMX, but I can't figure out how to install this extension. Downloaded the project from the link https://github.com/STMicroelectronics/x-cube-usb-pd . I was...

DalOpez by Associate II
  • 1523 Views
  • 2 replies
  • 0 kudos