STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why does HAL_QSPI_AutoPolling keep polling whereas the timeout has been reached and returning an error flag ?

Hello everyone,I'm today encountering a new issue where your help will be more than welcome.I'm communicating with an external Flash Memory using the QSPI of the STM32H7 than I own and everything is working as expected at the first run. I can write a...

0693W00000Ly1ApQAJ.png
DFell.1 by Associate II
  • 5378 Views
  • 9 replies
  • 2 kudos

AT+CEREG response is "+CEREG: 0,4", where 4 means "Unknown", even when connected to the Network. The modem is LBAD0ZZ1SE in stm32l462re board

I am currently working with TYPE1SE Modem (LBAD0ZZ1SE) in the stm32l462re board. I am having an issue where the modem response to the command AT+CEREG? is "+CEREG: 0,4", where 4 means "Unknown (for example, out of Evolved Terrestrial Radio Access Net...

SPere.2 by Associate III
  • 3320 Views
  • 1 replies
  • 0 kudos

I am used ethernet but facing issue

Hello there,I've recently switched on STM32 series of microcontrollers, to do so I've purchased STM32 Nucleo-H743ZI2 development board.My end application is based on Ethernet, so I am trying to get data from Ethernet but miserably failed. I’ve tried ...

Resolved! How to use a STM32G071B-DISCO Kit in SPY mode.

I have a STM32G071B-DISCO Kit. This device have a two USB C port. One is plug type and receptacle type. I'd like know how to use spy mode between SRC and SINK. I did connect this to SRC device and SINK device and connect micro-b port to STM32CubeMoni...

YKMIN by Associate II
  • 3005 Views
  • 3 replies
  • 0 kudos

Problems with FreeRTOS and lwIP Netconn API

Hello,I'am experimenting on using FreeRTOS in combination with lwIP. For that I am trying to rework some code by replacing lwIP's raw API with the netconn API. Now I am encountering two big problems:1: Using FreeRTOS with CMSIS V2:When setting up a n...

MLang.7 by Associate III
  • 2755 Views
  • 2 replies
  • 0 kudos