STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to create .wav file header ?

I am using stm32f7508-DK ,Working on audio recorder.c BSP example, <example working fine need to customize the example to meet our requirement>i want to created ( .wav) file based on incoming audio signal from microphones <U20 , U21 designator on Har...

Ss.61 by Associate III
  • 3007 Views
  • 2 replies
  • 0 kudos

Sending HTTP Post message to server with B-L462E-CELL1

Hello everyone,I'm not the best in programming (still learning ;) ) and am new to the B-L462E-CELL1. For my current project I need to send a HTTP POST message to a server. I have been struggling to do so. First I've tried to modify an example program...

AdVs by Associate
  • 1591 Views
  • 1 replies
  • 2 kudos

STM32F765 AND ATWINC1500

Hi All, I would like to implement a WiFi interface on a custom board based on the STM32F765.Until now I have been used wired ethernet interfaces. For the WiFi I plan to use an ATWINC1500 module connected with SPI. The module implements the stack ...

raffin by Associate III
  • 1338 Views
  • 0 replies
  • 1 kudos

UM0391, Is There A 2nd Testament?

Workalot is working on a DfuFileMgr 'look a like' (wdfufm if you will). It is to be embedded within a PC application.A first run through of 'wdfufm' establishes UM0391, 15-Feb-2007, sec 2.1, page 4 (aka 1st testament) misleads. In particular with th...

Workalot by Associate III
  • 863 Views
  • 0 replies
  • 0 kudos

STM32U585 serial programming (Embedded Linux)

Hi,Is there a way to program STM32U585 MCU via USART1 peripheral using Embedded Linux processor? Except BOOT0 pin and RESET pin of U5 MCU what else need to be done to get into Serial Programming mode? Thanks in advance,Nenad

NGajic by Associate III
  • 1998 Views
  • 2 replies
  • 0 kudos

usb host fat32 does not work with freeRTOS

I have stm32f429discovery and i used stm32cubeMx to set up usb host with fast32. when I connect flash it works OK. but when I configure freeRTOS it didn't work. when i debug it, I found it go to "HardFault_Handle" loop. i increase heap and stack size...

Javad by Associate III
  • 4032 Views
  • 5 replies
  • 1 kudos