User Activity

Hello,We use STM32F765VGT6 in our product. The datasheet says 1MB of flash memory available but it looks like there is 2MB available for use 0x0800 0000 to 0x081F FFFF. Is this a documentation issue? Can we use the extra 1MB flash starting from 0x081...
Hello, I see this in Errata es0334-stm32f76xxx."Host packet transmission may hang when connecting through a hub to a low-speed device"When the USB on-the-go full-speed peripheral connects to a low-speed device via a hub, the transmitter internalstate...
We have a situation on our stm32f765 running freeRTOS on one of our production ongoing avionic product. We see that with new lot of production units are hitting usage fault with INVPC status on USFR.Can some advice be provided on figuring out the las...
Kudos from
Kudos given to