STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 MW USB Host Library v3.4.0 release on GitHub

What is new in STM32 USB Host Library v3.4.0?*           Core driver :Fixes added to free RTOS resource during USB host DeInitCodeSpell and mcuAstlye fixesMultiple MisraC 2012 fixes*           All Classes :CodeSpell and mcuAstlye fixesMultiple MisraC...

STM32G0B1 USB PD NO UTILITY OS infinite loop.

When generating code with CubeMX for an USBPD sink application for the STM32G0B1 when no RTOS is used within the function USBPD_DPM_Run on line 340 till 363 it enters an inifinite do while loop. This happens in the usbpd_dpm_core.c file.It is undesir...

JBand.2 by Associate II
  • 1809 Views
  • 1 replies
  • 0 kudos

Unable to boot from bank2 with L073RZ

Hi,I have a simple application that I flashed to 0x0800 0000 and 0x0801 0000 using STM32CubeProgrammer. With BFB2 unchecked, the app runs correctly from bank1 but when I check BFB2 to boot from bank2 it looks like the board get stuck somewhere as the...

AlexS by Associate II
  • 1931 Views
  • 4 replies
  • 0 kudos

STM32F072R8 does not enter into DFU mode

Hello,I have custom board with STM32F072R8 and a USB interface to it. STM's USB is connected to USB of a x86 Board. STM as acting as USB device and x86 Board as USB host. When the board is powered up, I can see that STM is listed in the output of "ls...

ab_nurd by Associate II
  • 1404 Views
  • 2 replies
  • 0 kudos

Resolved! Unused pins to ground and bootloader question

Hello,I would like to put many pins on my UFBGA STM32 to ground, and configure in software as input or even better output( must be done correctly first time )But now I am wondering, if I am planning to BOOT processor with BOOT pin high, and use UART ...

0693W00000Lzai0QAB.png
Linas L by Senior II
  • 1472 Views
  • 2 replies
  • 1 kudos

Resolved! missing stm32f4xx_hal_uart.h in STM32F4xx_HAL_Driver

I recently go the 32F413HDISCOVERY board and downloaded the projects and examples to a local folder and imported it all of it into STM32CubeIDE.In the STM32CubeIDE I was able to open and modify the Test_001 project and blink LED2 and LED3. Next, I wa...

IMate.1 by Associate II
  • 5988 Views
  • 3 replies
  • 0 kudos

HAL QSPI AUTOPOLLING SUPPORT 4LINES?

I have read many samples in cube h7 github repository, and I have seen any hal autoplling example consulting status registers in 4 lines mode operation. It is supported? I am using STM32H750 with cube h7 1.10.0.

JCuna.1 by Senior
  • 2328 Views
  • 4 replies
  • 0 kudos

STM32G0B1KE System Bootloader Mode Entry

Hello ST Community,We are using STM32G0B1KE MCU in our project. The MCU firmware will be flashed from the Processor via the I2C interface between the processor and MCU.As per AN2606, we have tried to activate pattern 11, but the system bootloader cou...

Malik1 by Associate
  • 1904 Views
  • 3 replies
  • 0 kudos