STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

netXDuo TCP Server problem

Hello all. I'm writing an application with the NUCLEO-H563ZI board (with the intention to use later the STM32H563 into a custom board). My application will communicate with a master PC via the embedded Ethernet, exchanging process data and commands. ...

Resolved! i2c Error 4

Hi there !i work with DS2482 I2c to one wire . After i send the command reset i need the read the status register until i find one bit at 1, so i wrote my routine in this way  static uint8_t DS2482_Status_Register(void) { uint8_t register_status=0; ...

SGian.1 by Senior
  • 437 Views
  • 6 replies
  • 0 kudos

Resolved! Help with confguring STM32H7

CubeIDE: v2.0.0CubeMX: v6.16.1Debugger: ST-LINK/V2 V2J46S7Hello,I'm attempting to setup a dual core project using STM32H757XIH MCU on CubeMX. I've generated and imported the project for CubeIDE. I've configured the Trace and Debug -> DEBUG for "Seria...

schradz by Associate II
  • 272 Views
  • 4 replies
  • 0 kudos

STM32G491 and BOOT_LOCK

STM32G491KEU3 on custom board. Using STM32CubeProgrammer to read/change option bytes.With BOOT_LOCK unchecked I use STM32CubeIDE to flash and debug my project. However SysTick_Handler() is never called, so HAL_GetTick() always returns the same value ...