STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U5A9 USB MSC

  We are currently working on a project with the STM32U5 series running FreeRTOS and need to integrate the USB Mass Storage (MSC) class for adding pendrive / thumbdrive support. While exploring solutions, we noticed that CubeIDE doesn't directly supp...

nfkt by Associate
  • 971 Views
  • 1 replies
  • 0 kudos

Resolved! STM32N6 H264 video encoder and streaming over RTSP

Hello, I would like to know the H264 VENC performance for the STM32N6 using the ST example: STM32Cube_FW_N6_V1.1.1/Projects/STM32N6570-DK/Applications/VENC/VENC_RTSP_ServerI have a hardware setup with a nucleo-n657x0-q + a ST B-CAMS-IMX camera module...

FB__1 by Associate III
  • 2479 Views
  • 3 replies
  • 3 kudos

USB PD change voltage during active contract

Dear ST Community, I have a working application for USB PD SPR and EPR and now I want to change the voltage (power profile) during an active contract.So e.g. I have 5V currently and want to request 9V from the source, or I have 20V currently and want...

abtq by Associate III
  • 1181 Views
  • 8 replies
  • 2 kudos

Resolved! Output gain set is omitted in WM8904_Init()

Hi,// WM8904.c int32_t WM8904_Init(WM8904_Object_t *pObj, WM8904_Init_t *pInit) // ... if ((WM8904_CurrentDevices & WM8904_OUT_HEADPHONE) == WM8904_OUT_HEADPHONE) { ret += WM8904_SetVolume(pObj, VOLUME_OUTPUT, (uint8_t)pInit->Volume); } ...

ERROR by Senior
  • 237 Views
  • 2 replies
  • 1 kudos