STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! - Main Config: These peripherals still have some not configured or wrong parameter values: [CORTEX M7] getting error

Hello ,I am working on NUCLEO-H745ziq board. I am trying the example AZURE RTOS of Ux_CDC_device , the example provide in cubemx accordingly I setup the things in cubemx but when I try to generate the code it shows warning and the when I run the pro...

0693W00000QKISWQA5.png
MDeva.1 by Associate II
  • 5504 Views
  • 1 replies
  • 0 kudos

Is it possible to incorporate serial communication to a STM32L476 that is already defined as a USB Audio device?

I already define the nucleo-STM32L476 as a USB microphone, but I want to know if it is possible to communicate with the microcontroller trough serial communication. I want to implement these feature because I want to change the digital filters that I...

JacquiG29 by Associate II
  • 1521 Views
  • 1 replies
  • 0 kudos

STM32H747 and USB DISK - how to make it work?

Discovery board: STM32H747I-DISCO.OTG connected to P1 (HS).First of all, there are two modes:EXTERNAL PhyInternal FSEXTERNAL Phy is faster, Internal FS is slower. What does "external" mean?Will it just work or not?First I tried "Internal FS". Just do...

HTD by Senior III
  • 3786 Views
  • 6 replies
  • 0 kudos

Resolved! Are there any guides on how to include X-CUBE-USB-AUDIO functionality into an STM32CubeIde project (.ioc)?

Hello, I am looking to include USB audio streaming, this package looks perfect for handling a lot of the functionality. Just wondering if there are any guides on how to add this to a .ioc STM32CubeIde project for a different part than those in the Ex...

WFunk.1 by Associate
  • 1862 Views
  • 1 replies
  • 0 kudos

Project with STM32CubeExpansion_CELLULAR_V7.0.0 and STM32CubeExpansion_Cloud_AZURE_V2.0.0 under STM32CubeAzureRTOS

We have a project where we want to exchange sensor data between our battery powered device and the AZURE cloud through a mobile network. For developing we use the P-L496G-CELL02 board with the BG96 modem attached.So it's similar to the (very old) STM...

MiEx13 by Associate II
  • 785 Views
  • 0 replies
  • 1 kudos

Question about STM32 MCU that does not perform the program on it's flash memory, after turning it off, and then on.

Hi, I'm using STM32 MCU: STM32L4A6AGIxP.The IDE that I use to write the code for the MCU is: STM32CubeIDE v1.10.1.The BOOT0 pin of this MCU is floating and not connected to GND.The big problem that the MCU is SMT FBGA type and and soldered to the PCB...

REldo.1 by Associate II
  • 5596 Views
  • 10 replies
  • 0 kudos