STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Advice on getting STM32 CAN bus to PC

Some time ago I designed a simple CAN to USB device. It accepts CAN network packets, then converts them to a binary packet that is sent to the virtual COM port. It works very well. However, the Virtual COM Port is limited to about 1MB/s even thou...

Apparent minor bug in HAL_TIM_IRQHandler()

There appears to be a minor bug in HAL_TIM_IRQHandler(), in stm32f7xx_hal_tim.chttps://github.com/STMicroelectronics/STM32CubeF7/blob/master/Drivers/STM32F7xx_HAL_Driver/Src/stm32f7xx_hal_tim.cAPPARENT-BUG SUMMARY:There's a line-of-code that works, b...

JimYuill by Associate II
  • 2918 Views
  • 5 replies
  • 1 kudos

Hello All, I am using STM32f105rbt, issue is comming when i am using Ethernet and PWM using TIM1 simualteniously. individually both are working. please any one can help me?

If i am generating PWM pulse by uing TIM1 (PA8) my ethernnet not worming? for ethernet config i m using CMSIS lib provided by STPwm configuration is s follows RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph...

Shail by Associate II
  • 1381 Views
  • 1 replies
  • 0 kudos

STM32F7 record SPDIF data to SD card

Hi,​I'm trying to use a STM32F746 to record SPDIF_Rx to SD card. I'm already got some data and save to SD card.​I use HAL_SPDIFRX_ReceiveDataFlow_DMA(&hspdif, (uint32_t*)&BufferCtl.pcm_buff_32[0], AUDIO_IN_PCM_BUFFER_HALF_SIZE)and HAL_SPDIFRX_RxHalfC...

庭張.1 by Associate
  • 1138 Views
  • 0 replies
  • 0 kudos