STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Filex writing performance

Hello everyone, I am using a custom board with STM32H750 and I am trying to develop a file system with FILEX. The file system' s media is a uSD card with 10 MB/s baudrate which is communicating with the micro thanks to the SDMMC peripheral. The SDMMC...

FCola.1 by Associate III
  • 1795 Views
  • 4 replies
  • 4 kudos

Resolved! USB CDC and USART recommended practice

When using USB CDC to communicate via USART, and interacting with USART data, in code is it recommended to interact with it at the USB side, or to interact with it at the USART side?From what I can tell, both offer both polling and interrupt methods....

Resolved! Closing STM32H533 debug ports with no TZ enabled

Hello,in our application, running on a H533RET6 and with no TZ enabled, we need to close debug ports in production.I preliminarly did some tests using CubeProgrammer: I generated password-based credentials (obk+bin files, which as far as I understand...

ste2108_0-1769514352577.png ste2108_1-1769514604852.png ste2108_2-1769516015931.png
ste2108 by Associate II
  • 348 Views
  • 2 replies
  • 1 kudos

STM32H503RB I3C private communication(read)

Hello everyone, I'm having some trouble implementing I3C communication and would like to ask for some help.   I am using the NUCLEO-H503RB board as my main controller. For the target devices, I have the NUCLEO-IKS01A3 expansion board and the TSC1641 ...

roro_0-1769757273958.png roro_1-1769757273943.png
roro by Associate
  • 204 Views
  • 0 replies
  • 0 kudos