STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-STM32F767ZI and STM32 CUBE IDE

Good day,I have a NUCLEO-STM32F767ZI and a problem with the STM32 CUBE IDE. When I create a project in version 1.5.1 with ETH, FreeRTOS and LWIP everything works fine. When I create the same thing in the latest version, the generated code falls into ...

DJeze.1 by Associate II
  • 2887 Views
  • 4 replies
  • 0 kudos

Why is remapping necessary for jumping to bootloader?

When jumping to bootloader from software for devices such as the stm32l4, why is it necessary to remap system memory to address 0x0000 0000 in address space by calling __HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH? On the contrary, the stm32H7 doesn't require...

AC.1 by Associate II
  • 3707 Views
  • 6 replies
  • 0 kudos

Example on MOOC about RTOS tickles doesn't works.

I am following an the example from MOOC;https://www.youtube.com/watch?v=nSLN_WM2TOc&list=PLnMKNibPkDnExrAsDpjjF1PsvtoAIBquX&index=59&t=889sI can't make it work, apparently LPTIM trigger interrupts continuously.I create a fresh project to reproduce pr...

0693W00000WK1zXQAT.png
dhs by Senior
  • 896 Views
  • 0 replies
  • 0 kudos

Issue detecting and processing usart receive

Hello again,Here's what I want to do:1) wait for the UART_FLAG_RXNE to be set2) receive one character3) switch based on that character (character is saved for further processing)4) receive the proper number of following characters based on the comman...

Where does Bootloader for STM32G0B1M1 look for a USB cable? My previous question was how to detect a USB cable, but the answer was just use VBUS and an EXTI to detect. Which interrupt does the bootloader monitor for a cable?

My previous question was how to detect a cable and they said to use a EXTI to receive a VBUS detection. The customer wants to use USB to program a blank device (so nothing configured) and EXTI is a block of interrupts and could be multiple pins. Ple...

SMoor.1 by Associate II
  • 2022 Views
  • 4 replies
  • 0 kudos

Unable to get B-L072Z-LRWAN1 into DFU mode

I'm wondering if i'm missing something here.I've hooked up BOOT0 to the 5V pin on CN2. I have nBOOT1 set to 1, and i'm connected to the device via the ST-LINK as the other usb port doesn't seem to be active. I've also installed the udev rules, and ju...

SBurs.1 by Associate II
  • 2741 Views
  • 6 replies
  • 0 kudos

Lost some data when send to PC with USB.

HI all,I need a sampling rate of 1K to collect the analog voltage.My chip is :STM32F103C8T6.I use Timer2's interrupt to enable collect and send data, after send disable.I use a plus at 100Hz to verify, find it will lost some data:ThanksBoone

0693W00000UnZyEQAV.png 0693W00000Una0eQAB.png
BLu.1 by Associate II
  • 1415 Views
  • 2 replies
  • 0 kudos