STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is there a difference between TX_APP_MEM_POOL_SIZE in the app_azure_rtos_config.h and APP_BYTE_POOL_SIZE in app_threadx.h when using ThreadX?

I have created an application using CubeMX inside CubeIDE and setting the ThreadX memory pool size in CubeMX sets the value generated in the app_azure_rtos_config.h. CubeMX also generates app_threadx.c and app_thread.h, but in app_threadx.h most exa...

USB-HS (ULPI) on STM32H750

Hi,is somebody operating the STM32H750 successfully with USB-HS (ULPI Interface)?I succeeded in running the USB device CDC example of the STM32H743 evaluation board on my STM32H743 test board (144 pin LQFP) - but when I try the same with a test board...

flyer31 by Senior
  • 10365 Views
  • 14 replies
  • 2 kudos

Resolved! Warning with ThreadX Source path

Why am I seeing the warning:Invalid project path: Missing project folder or file: /STM32H743-EVAL-Utils/ThreadX for Source path.the source folder the warning is complaining about is not visible while browsing the project folder. It is not visible whe...

Implementing separate power supply for IWDG (watchdog)

HiIn the STM32H7 dual-core safety manual (UM2840) Section 4.2.1 Power supply, ST states that it is recommended to use a separate power supply for IWDG. In the reference manual (RM0399) in figure 576 it is displayed that IWDG is supplied from Vdd doma...

Itchy by Associate II
  • 3368 Views
  • 5 replies
  • 0 kudos