STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F446RCT6 this is the IC I am working on and which has 256kb flash, I didn't got a proper data sheet of the same

Hi I am a new bee here, I wanted to create a bootloader to flash two applications, so i need the flash partitions which I didn't got in the datasheet properly.and also I wanted to implement OTA so is this STM32F446RTC6 is capable of all this????

SBhat.5 by Associate II
  • 3826 Views
  • 8 replies
  • 0 kudos

STM32F303 USB CDC tutorial

Hello,I am trying the USB Communication stm32f303 with android phone usins CDC USB TERMINAL app . I am able transmit all the string. But while reception I am receiving only the first character.

Resolved! STM32F4x HAL_ETH_ReadPHYRegister blocking mode

Dear allAfter having enabled ETH + LwIP stack we are experiencing that something in the init phase are keeping blocked all.After a while we see that the root causes is inside HAL_ETH_ReadPHYRegister.Specifically we are referring at this part of code:...

0693W00000GXG4xQAH.png