STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL_UART functions do not work with Azure RTOS ThreadX

Hello,I followed this guide:https://community.st.com/s/article/how-does-the-threadx-semaphore-workAnd everything works.But when I try to add a modification, a HAL_UART_Transmit - HAL_UART_Transmit(&huart2, (uint8_t *)&message, 1, 10); - in one thread...

MStew.1 by Associate III
  • 4133 Views
  • 6 replies
  • 0 kudos

Resolved! Question about the Azure RTOS ThreadX Semaphore example

Hello,in the Semaphore example(https://community.st.com/s/article/how-does-the-threadx-semaphore-work) there is this step:Open Core\Src \main.c – you can copy and paste the code below, but please notice the" USER CODE BEGIN", to properly place the co...

MStew.1 by Associate III
  • 2622 Views
  • 3 replies
  • 0 kudos

Driver for ksz8863 switch?

Hi, does ST have it's own driver implementation of the ksz8863 switch. If yes where can i download it. I like to have an link up/down feedback. Need to have connection to the internal register of that switch. For now i just use the lan8742 driver pro...

MOtto.2 by Associate II
  • 5705 Views
  • 4 replies
  • 1 kudos

Resolved! custom bootloader problem on STM32F405

helloi am working on a custom bootloader or STM32F405.the Flash process is done correctly by the Bootloader, i checked the content of the flash.the problem happens when the bootloader jumps to the application firmware which is located at adress 0x080...

0693W00000aHet4QAC.jpg 0693W00000aHetPQAS.jpg
ZTale.1 by Associate II
  • 5628 Views
  • 10 replies
  • 0 kudos

Resolved! SDCard (SDIO) connector on stm32f723e-disco

Hi all,is it possible to connect a SDCard to the stm32f723e-disco [1] board? The webpage [1] is talking about some microSD connector, but I do not really find one. So is this a mistake on the webpage?Additionally, I would like to ask, if it is possib...

whati001 by Associate II
  • 1486 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H725 supports VCP over USB?

Hello,i am porting a project made initially on STM32H750, but because of the semiconductor shortage on the market, the only available part was a stm32H725IGK6, which i started working on.Regarding the usb connection, i have the following pins used:P...

Bogdan by Senior
  • 2105 Views
  • 3 replies
  • 0 kudos

How do i use HAL_UART in AZURE RTOS

Hi i would like to have an example code or something that helps me out, I wanna know how to use HAL functions in AZURE RTOS ,When i try to use HAL_UART_TRANSMIT(&huart2,pdata,size,timeout) i get an error that huart is not defined like wise same for P...

SC.J.1 by Associate
  • 1497 Views
  • 2 replies
  • 0 kudos

Resolved! The callback function HAL_DAC_ConvCpltCallbackCh1(DAC_HandleTypeDef* hdac) with STM32U575CGU6 doesn't work

Could someone assist and clarify how to configure GPDMA for DAC for use the callback function HAL_DAC_ConvCpltCallbackCh1(DAC_HandleTypeDef* hdac) with STM32U575CGU6. I caught:/* Data Transfer Error Interrupt management */ if ((__HAL_DMA_GET_FLAG(hdm...

Pavel D by Associate II
  • 5932 Views
  • 6 replies
  • 0 kudos