STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Getting timestamps for transmitted PTP datagrams

Hi,I am implementing PTP slave on bare metal H743II with firmware 1.12.1 and LwIP 2.1.2.Timestamps for transmitted PTP datagrams can be received by implemented a callback function HAL_ETH_TxPtpCallback(). The callback is called from stm32h7xx_hal_eth...

edgarj by Associate
  • 268 Views
  • 1 replies
  • 1 kudos

X-CUBE Audio support for STM32H7

Hi Michel    I am working on an Audio project using STM32H7A3VGH6 and STM32H743VGH6.  I am interested in rate conversion from 44.1K to 48K ( I have a float version ) in Int16 and the Multi band DRC mentioned above.  I did find the SRC441 in the X-Cub...

SChak.1 by Associate
  • 325 Views
  • 3 replies
  • 0 kudos

stm32g491 flash dual bank support

Hi,I’m currently working on the STM32G491 series MCU. Our requirement is to support OTA firmware upgrades. In case the flashing process fails, the system should automatically revert to the previous firmware.Does the STM32G491 support this feature by ...

STM32U5 with DMA request AND trigger.

I have GPDMA working on STM32U5 with a circular buffer.  However, when I add a GPDMA "trigger" to the setup, the DMA no longer works. GPDMA1_C2TR2.TRIGPOL=2 GPDMA1_C2TR2.TRIGSEL=11 GPDMA1_C2TR2.TRIGM=3 LPTIM1 setup to clock away at a 50% duty cycle. ...

STM32H7S3V8T6 timer triggered DMA

Hi All, Trying to setup timer triggered DMA for the STM32H7S3V8T6 micro and cannot seem to get it workingI have tried a number of things and eventually resorted to asking chatGPT but so far no dice... What I want to achieve1. Timer 1 toggles CH1 outp...

JShro by Associate III
  • 418 Views
  • 1 replies
  • 0 kudos