cancel
Showing results for 
Search instead for 
Did you mean: 

Split data from a float array into an uint8_t array

some_guy
Associate

Hi,

I just stumbled upon something interesting (at least for me). For my current project I need to store data from a float array with two elements in an uint8_t array with eight elements. I use the following code to archive this:

pnt = (uint8_t*)out;
for(i = 0; i < 8; i++)
{
    uart_tx_buffer[i + 3] = *(pnt + i);
}

While it technically works, the bytes from each float element get stored in the buffer in a reversed order. I can give you an example from what I am looking at in the debug session. The float array has the values out = {0x41bef708, 0x4478a1d7}. So the result I exacted for the buffer is uart_tx_buffer = {xx, xx, xx, 0x41, 0xbe, 0xf7, 0x08, 0x44, 0x78, 0xa1, 0xd7}. But in reality it looks like this uart_tx_buffer = {xx, xx, xx, 0x08, 0xf7, 0xbe, 0x41, 0xd7, 0xa1, 0x78, 0x44}.

At first I thought the values in the buffer are completely random because I made a mistake. It took me a while to figure this out. What is the reason why this happens? Can I avoid this, because now I would have to shift all these bytes around.

I am using STM32CubeIDE 1.19.0 to program a NUCLEO-F429ZI.

2 REPLIES 2
Ozone
Principal III

This issue is called endianness, and refers to an architecture's way of storing and accessing objects greater than 1 byte (usually the minimal size for an object in memory).
https://en.wikipedia.org/wiki/Endianness
If it comes to communication between different systems, either use ASCII/text format, or stick to one endianness. 
As an example, CANopen defines "Little Endian" for all message transfers.

TDK
Super User

If you want the same memory order, use memcpy.

uint8_t one[8];
float two[2];
memcpy(two, one, 8);

If byte order needs swapped, you can use __REV to reverse endianness: 

uint8_t one[8];
float two[2];
two[0] = __REV(((uint32_t*)one)[0]);
two[1] = __REV(((uint32_t*)one)[1]);

 

If you feel a post has answered your question, please click "Accept as Solution".