cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE Audio support for STM32H7

SChak.1
Associate

Hi Michel 

  I am working on an Audio project using STM32H7A3VGH6 and STM32H743VGH6.  I am interested in rate conversion from 44.1K to 48K ( I have a float version ) in Int16 and the Multi band DRC mentioned above.

 I did find the SRC441 in the X-Cube-Audio libray though the documentation mentions support for the STM32F series.

 Hope this will work for the H series as well.

 

 I did not find the MB-DRC though there is a SVC code.  Is this the same as MB-DRC ( the document seems to indicate it as a single band only ).  Is there a link where I can get the code for this ?

 

Rgds

Edit: Moved from X-CUBE-AUDIO-KIT Audio Latency

3 REPLIES 3
Saket_Om
ST Employee

Hello @SChak.1 

I reported your question internally. We will get back to you as soon as possible. 

Internal ticket number: 220518 (This is an internal tracking number and is not accessible or usable by customers).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om
MichelM
ST Employee

Hello @SChak.1

 

Regarding SRC441 library, I am not the right guy to know if it works on your platform; I forwarded your question to the right person.

Regarding MDRC, it is part of x-cube-audio-kit (it is not available as a library), it is not inside x-cube-audio library; VLC which is inside x-cube-audio library is a simpler algorithm which may perhaps fulfill your requirement (but it is not multi-band).


Michel

Hello @MichelM and @SChak.1,

Regarding SRC441 library, there already are the Cortex-M7 binaries so it should work on STM32H7 boards.

Best regards,

Petr